Wiki

This version is outdated by a newer approved version.DiffThis version (07 May 2021 13:42) was approved by Prasad Kamath.The Previously approved version (19 Mar 2021 14:55) is available.Diff

This is an old revision of the document!


Click here to return to the IO page

Interface Read



Description


The Interface Read block takes value from one of eight interface registers and makes it available in the schematic design. The yellow pin can connect to GPIO Conditioning block's yellow input pins. It is especially useful for parts that self-boot and use external interface registers.


Usage


Select a particular interface from the drop-down.

  • Every input must be connected to an output, else there will be errors on compilation.
  • Observe that as you drag more output blocks to your schematic, your number of interfaces available decreases.

Note: This block is only available for DSPs with GPIOs or auxiliary ADC.

Targets Supported

NameADSP-214xxADSP-215xx/ADSP-SC5xxADAU145x/1456x
—————————————-——————————————————————————————--——————————————-
Interface Read Not supported Not supported Sample


Pins

Output

NameTypeDescription
———————————-———————--
InterfaceRead LogicInterface read output channel


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
—————————————- ———————- ————————————- —————————————-
SelectedIFIPChannelINTFACE_0 INTFACE_0 to INTFACE_7 Selects the Interface Read channel


DSP Parameters

Parameter NameDescriptionADSP-214xx/SC5xx/215xxADAU145x/ADAU146x
—————————-- ———————————— —————————————————-- ———————————--

Not applicable


DSP Parameter Computation

Not applicable

resources/tools-software/sigmastudiov2/modules/inputoutput/interfaceread.1620387704.txt.gz · Last modified: 07 May 2021 13:41 by Prasad Kamath