Wiki

This version (18 May 2021 09:01) was approved by John Joseph.The Previously approved version (05 May 2021 13:00) is available.Diff

Click here to return to the IO page

Input


Description

The Input block receives input from the hardware's input pins and makes it available in the schematic design.

Usage

Check the block for the input channel(s) you with to enable. Un-check the box disable an input channel. The pin will turn blue when an input is enabled and grey when disabled. The default block has two pins enabled, for stereo connection.

Every enabled input must be connected to an output, else there will be errors on compilation. Only a single input block can be associated with a processor. You will receive an error if you attempt to add multiple inputs to a schematic. To change the Input's Sampling Rate, Right-click the block name and select Set Sampling Rate, which will open the Sampling Rate window (default is 48 kHz):

Targets Supported

NameADSP-214xxADSP-215xx/ADSP-SC5xx ADAU145x/ADAU146x
————————————————-——————————————-——————————--
Input Block & Sample Block & Sample Sample


Pins

Output

NameTypeDescription
——————————-————————————-—————————--
Output0AudioOutput channel 0
Output1AudioOutput channel 1


Configurable Parameters


Not applicable

DSP Parameters

No DSP Parameters

resources/tools-software/sigmastudiov2/modules/inputoutput/input.txt · Last modified: 13 May 2021 09:34 by Prasad Kamath