Wiki

This version (18 May 2021 09:01) was approved by John Joseph.The Previously approved version (06 May 2021 08:05) is available.Diff

Click here to return to the IO page

ASRC Output


Description

The ASRC Output block routes signals between the schematic design and the hardwares ASRCs (Asynchronous Sample Rate Converters).

These blocks are only available for use with DSPs that have integrated ASRCs.


Usage

Use the output block's drop-down list control to select from the available ASRCs.

  • Every ASRC Output must have its input connected, else there will be errors on compilation.
  • Observe that as you drag more ASRC output blocks into the schematic, the number of available outputs in the drop-down decreases because they can only be represented by one block at a time.


Targets Supported

NameADSP-214xxADSP-215xx/ADSP-SC5xxADAU145x/ADAU146x
————————-——————————————————————--———————————-
ASRC Output Not available Not available Sample


Pins

Input

NameTypeDescription
——————————--——————————————————-——————————————————————-
input AudioOutputs the audio to the hardware pin


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
——————————————-———————-——————————--—————————————-
SelectedASRCOPChannel0 0 to 15 Selected output channel


DSP Parameters


Not applicable

resources/tools-software/sigmastudiov2/modules/inputoutput/asrcoutput.txt · Last modified: 12 May 2021 13:23 by Prasad Kamath