This is an old revision of the document!
Click here to return to the Filters page
Tracking Filters are useful for dynamic shifting of filtering. The tracking filter allows for the centre frequency to be determined by an external input .
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
Tracking Filter | No | Yes | No | Yes |
Name | Type | Description |
---|---|---|
Input | Audio | Input Signal |
NormalizedCentreFrequency | Control | Control Input |
Name | Type | Description |
---|---|---|
FilteredOutput | Audio | Filtered Output Signal |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
Gain | 0 | -15dB to 15dB | Gain of the filter in DB |
QValue | 1.71 | 0 to 16 | Quiscent value of the filter |
Boost | -15 | -15dB to 15dB | Filter boost value in DB |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx |
---|---|---|
GainLin | Array of coefficients | Float Array |