Wiki

The most recent version of this page is a draft.DiffThis version (17 Feb 2021 04:58) was approved by John Joseph.

This is an old revision of the document!


Click here to return to the Filters page

Non-Bare Filter

Description

NonBare filters are second order filters which take the parameters directly. The filter parameters are converted to filter coefficients by the Module itself. Regalia-Mitra algorithm is used for this implementation.

Targets Supported

NameADSP-214xx(Sample)ADSP-214xx(Block)ADSP-215xx/ADSP-SC5xx(Sample)ADSP-215xx/ADSP-SC5xx(Block)
Non-Bare Filter No Yes No Yes


Pins

Input

Name Type Description
InputAudioInput Channel

Output

Name Type Description
OutputAudioOutput channel


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
Gain 0dB -15 to 15dB Gain of the filter in DB
Qvalue 1.71 0.04 to 16 Quiscent factor of the filter
K 1 0.04 to 16 K values as described in the algorithm
Frequency 1000 1 to 24000 Hz Cut-off frequency of the filter


DSP Parameters

Parameter NameDescriptionADSP-214xx/SC5xx/215xx
Frequency Cut-off frequency of the filter Float
Omega Quiscent factor of the filter Float
Gain Gain of the filter in DB Float
K K values as described in the algorithm Float
/srv/wiki.analog.com/data/pages/resources/tools-software/sigmastudiov2/modules/filters/nonbarefilter.txt · Last modified: 13 May 2021 14:56 by Sreesha Y M