This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:tools-software:sigmastudiov2:modules:filters:dcblocking [05 Feb 2020 08:05] – Added an image Sanjeeva Reddy | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | [[resources/ | ||
+ | ====== DC Blocking ====== | ||
+ | \\ | ||
+ | {{: | ||
+ | ===== Description ===== | ||
+ | The DC Blocking filter blocks the direct components in the input signal and sends the output signal without DC component. | ||
+ | |||
+ | The dc-blocking behavior is computed according to the following transfer function: | ||
+ | |||
+ | H(z) = (1 - z^-1)/(1 - Rz^-1) | ||
+ | |||
+ | Note: R = 0.9999 which is a cutoff frequency of 0.1Hz at 48kHz. | ||
+ | \\ | ||
+ | ===== Targets Supported ===== | ||
+ | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | ||
+ | |DCBlocking| Yes | Yes|Yes| Yes| | ||
+ | \\ | ||
+ | ===== Pins ===== | ||
+ | ==== Input ==== | ||
+ | ^Name^Type^Description^ | ||
+ | |Input|Audio|Input Channel 0| | ||
+ | ==== Output ==== | ||
+ | ^Name^Type^Description^ | ||
+ | |DCBlocked_Signal|Audio|Output channel 0| | ||
+ | \\ | ||
+ | ===== Configurable Parameters ===== | ||
+ | No configureable parameters | ||
+ | \\ | ||
+ | ===== DSP Parameters ===== | ||
+ | No DSP parameters | ||
+ | \\ | ||