This is an old revision of the document!
Click here to return to the Filters page
The Crossover block includes 2-way and 3-way crossover filters, typically used in loudspeaker systems to split the audio signal into separate frequency bands.
This filter provides:
2-way or 3-way crossover filtering.
Graphical design of crossover response.
Selectable crossover types: Linkwitz-Riley, Butterworth, Bessel.
Selectable filter orders: 2nd, 3rd, 4th, 6th, and 8th
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
—————————- | ——————-- | ——————————-- | —————————- |
Crossover 3 Way | NA | B/S | S |
Crossover 2 Way | NA | B/S | S |
Name | Type | Description |
---|---|---|
———————————-- | —————————— | ————————————-- |
Input0 | Audio | Input Channel 0 |
Name | Type | Description |
---|---|---|
———————————————————-- | —————————— | ———————————————— |
Output0 | Audio | Output channel 0 |
Output1 | Audio | Output channel 1 |
Output2 (CrossOver 3 Way Only) | Audio | Output channel 2 |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
————————————— | ————————— | ——————————————— | ———————————————————- |
LowFrequency | 250 | 3 to 30 KHz | Cut-off frequency for Low Filter |
MidLowFrequency | 250 | 3 to 30 KHz | Cut-off frequency for Mid-Low filter |
MidHighFrequency | 3000 | 3 to 30 KHz | Cut-off frequency for Mid-High Filter |
HighFrequency | 3000 | 3 to 30 KHz | Cut-off frequency for High Filter |
LowGain | 0 dB | -10 to +10 dB | Filter Gain for Low Filter |
MidLowGain | 0 dB | -10 to +10 dB | Filter Gain for Mid-Low Filter |
MidHighGain | 0 dB | -10 to +10 dB | Filter Gain for Mid-High Filter |
HighGain | 0 dB | -10 to +10 dB | Filter Gain for High Filter |
LowFilterType | Linkwitz-Riley | Filters List | Used to select the filter type for Low Filter |
MidLowFilterType | Linkwitz-Riley | Filters List | Used to select the filter type for Mid-Low Filter |
MidHighFilterType | Linkwitz-Riley | Filters List | Used to select the filter type for Mid-High Filter |
HighFilterType | Linkwitz-Riley | Filters List | Used to select the filter type for High Filter |
LowInvertPolarity | False | True/False | Invert polarity of Low Filter |
HighInvertPolarity | False | True/False | Invert Polarity of High Filter |
LinkLowMidFilters | False | True/False | Link the low and mid low filters to ensure frequency changes in the two filters are same |
LinkMidHighFilters | False | True/False | Link the high and mid high filters to ensure frequency changes in the two filters are same |
Note : Mid Low and Mid High filters and their parameters are only applicable for Crossover 3 Way Filters.
Parameter Name | Description | ADSP-214xx/SC5xx/215xx | ADAU145x/146x |
---|---|---|---|
———————————— | ———————————————————————————————— | —————————————- | —————————- |
LowPolarity | Polarity Inversion Status of Low Filter | FixInt32 | FixInt32 |
HighPolarity | Polarity Inversion Status of High Filter | FixInt32 | FixInt32 |
LowFilterCount | Number of bi-quads for Low Filter Type | FixInt32 | FixInt32 |
MidFilterCount | Number of bi-quads for Mid Filter Type | FixInt32 | FixInt32 |
HighFilterCount | Number of bi-quads for High Filter Type | FixInt32 | FixInt32 |
A1_FilterType | Filter coefficient A1 of bi-quad stage X Mid/Low/High FilterType | Float | Float |
A2_FilterType | Filter coefficient A2 of bi-quad stage X Mid/Low/High FilterType | Float | Float |
B0_FilterType | Filter coefficient B0 of bi-quad stage X Mid/Low/High FilterType | Float | Float |
B1_FilterType | Filter coefficient B1 of bi-quad stage X Mid/Low/High FilterType | Float | Float |
B2_FilterType | Filter coefficient B2 of bi-quad stage X Mid/Low/High FilterType | Float | Float |
Note FilterType Refers to Low, Mid-Low, Mid-High and High.