Wiki

This version (18 May 2021 08:59) was approved by John Joseph.The Previously approved version (08 Feb 2021 06:19) is available.Diff

Click here to return to the Dynamic Processors page

RMS Compressor with Max/Avg IP

Description

This Module computes the Gain of the Compressor. Compression happens by taking the RMS of the Average or Max of all inputs, and then looking up for the Gain based on the Compressor Graph.

Targets Supported

Name ADSP-214xx ADSP-215xx/SC5xx ADAU145x/146x
——————————————————-- —————————- ——————————-- —————————-
RMS Compressor with Max/Avg B B NA


Pins

Input

NameTypeDescription
————————————— —————————— ————————————————
Input Audio Input channel

Output

NameTypeDescription
————————————— —————————— ————————————————
Output ControlCompressor Gain


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
———————————————- —————————- ————————————- —————————————————————-
RMSTC 121 1 – 8686 db/s Determines how rapidly the compressor will respond to input signal level changes
Hold 0 0-2000 Controls the time (in ms) the compressor maintains its current output gain setting before it starts decreasing as the input level decrease.
Decay 10 1 - 8686 db/s Controls the rate at which the compressor gain decreases in response to decrease in the input signal level.
Soft-knee - - Soft-knee lets the compressor ease into action, making a less-abrupt change from unprocessed signal to compressed signal.
Graph - - Compression Editor Graph.


DSP Parameters

Parameter NameDescriptionADSP-214xx/SC5xx/215xx
—————————— ———————————————-- ——————————————-
RMSTC RMS Time Constant Float
Decay Decay Float
Hold Hold Float
Graph Compressor Graph table values Float Array


resources/tools-software/sigmastudiov2/modules/dynamicsprocessors/rmsipmaxavg.txt · Last modified: 12 May 2021 09:38 by John Joseph