Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:sigmastudiov2:modules:dynamicsprocessors:peakwithexternaldetectorinput [15 Jan 2021 11:07] – [Peak w/Ext Detector] Nikhin Shettyresources:tools-software:sigmastudiov2:modules:dynamicsprocessors:peakwithexternaldetectorinput [12 May 2021 09:36] (current) John Joseph
Line 1: Line 1:
-[[resources/tools-software/sigmastudiov2/modules/dynamicprocessors|Click here to return to the Dynamic Processors page]]+[[resources/tools-software/sigmastudiov2/modules/dynamicsprocessors|Click here to return to the Dynamic Processors page]]
 ====== Peak w/Ext Detector ====== ====== Peak w/Ext Detector ======
 \\ \\
Line 7: Line 7:
 ===== Description ===== ===== Description =====
 The Peak w/Ext Detector Compressor block computes the peak level of the control signal, if peak of the signal is more than threshold, signal level is changes to new peak level and if the peak level is below the threshold level, it slowly reaches reaches the new peak level by accounting the hold and decay time. The Peak w/Ext Detector Compressor block computes the peak level of the control signal, if peak of the signal is more than threshold, signal level is changes to new peak level and if the peak level is below the threshold level, it slowly reaches reaches the new peak level by accounting the hold and decay time.
 +\\
 +===== Variants =====
 +  - Peak w/Ext Detector
 +  - Peak w/Ext Detector with Gain Out
 +
 \\ \\
 ===== Targets Supported ===== ===== Targets Supported =====
-^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ADSP-SC5xx(Sample)^ADSP-215xx/ADSP-SC5xx(Block)+^ Name             ^ ADSP-214xx ^ ADSP-215xx/SC5xx ^ ADAU145x/146x ^ 
-|Peak w/Ext Detector| Yes Yes|YesYes|+| -------------------------------------------------------- | ---------------------------- | -------------------------------- | ---------------------------- | 
 +| Peak w/Ext Detector | B/S        B/S              S           | 
 +Peak w/Ext Detector with Gain Out | NA        | NA              | S           | 
 \\ \\
 ===== Pins ===== ===== Pins =====
 ==== Input ==== ==== Input ====
 ^Name^Type^Description^ ^Name^Type^Description^
 +| --------------------------------------- | ------------------------------ | ------------------------------------------------ |
 |ExtDetectorInput|Control|Peak input for the compressor| |ExtDetectorInput|Control|Peak input for the compressor|
 |Input1|Audio|Input channel1| |Input1|Audio|Input channel1|
 ==== Output ==== ==== Output ====
 ^Name^Type^Description^ ^Name^Type^Description^
 +| --------------------------------------- | ------------------------------ | ------------------------------------------------ |
 |Output1|Audio|Output channel1| |Output1|Audio|Output channel1|
 \\ \\
 ===== Configurable Parameters ===== ===== Configurable Parameters =====
 ^GUI Parameter Name^Default Value^Range^Function Description^ ^GUI Parameter Name^Default Value^Range^Function Description^
 +| ----------------------------------------------               | ----------------------------        | ------------------------------------- |---------------------------------------------------------------- |
 |Hold|0 ms|0 to 2000 ms|Controls the time (in ms) the compressor maintains its current output  gain setting before it starts decreasing as the input level decrease.| |Hold|0 ms|0 to 2000 ms|Controls the time (in ms) the compressor maintains its current output  gain setting before it starts decreasing as the input level decrease.|
 |Decay| 10 dB/s| 0 to 10000 dB/s|Controls the rate at which the compressor gain decreases in response to decrease in the input signal level, e.g. the “Release” time.| |Decay| 10 dB/s| 0 to 10000 dB/s|Controls the rate at which the compressor gain decreases in response to decrease in the input signal level, e.g. the “Release” time.|
Line 31: Line 42:
 \\ \\
 ===== DSP Parameters ===== ===== DSP Parameters =====
-^Parameter Name^Description^ADSP-214xx/SC5xx/215xx^ +^Parameter Name^Description^ADSP-214xx/SC5xx/215xx^ ADAU145x/146x ^ 
-|Hold|Hold value|Float| +|------------------------------ |------------------------------------------ |-------------------------------------------| ---------------------------------------------- | 
-|Decay|Decay value|Float| +|Hold|Hold value|Float| 8.24 format
-|Table|Table values | Float|+|Decay|Decay value|Float| 8.24 format
 +|Table|Table values | Float| 8.24 format|
 \\ \\
 ===== DSP Parameter Computation ===== ===== DSP Parameter Computation =====
resources/tools-software/sigmastudiov2/modules/dynamicsprocessors/peakwithexternaldetectorinput.txt · Last modified: 12 May 2021 09:36 by John Joseph