This is an old revision of the document!
Click here to return to the Basic page
The Multi-Tap Voltage Controlled Delay cell provides a variable delay to a single audio input, producing multiple outputs. Each output signal is called a “tap.” The amount of delay for each tap can be modified in real-time by updating the value on the corresponding control input pin.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
VolatgeControlledDelay | Yes | Yes | Yes | Yes |
Name | Type | Description |
---|---|---|
Input0 | Audio | Input channel0 |
DelayTap0 | Control | Current delay for Output channel0 |
Name | Type | Description |
---|---|---|
Output0 | Audio | Output channel0 |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
MaxDelay | 1 | 1 to 1500 (Depends on Size of the Memory available) | Controls the maximum amount of delay that can be used for each output tap. Change in this value requires a re-compilation |
NumChannels | 1 | 20 | Number of DealyTap and Output channels. Change in this value requires a re-compilation |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx |
---|---|---|
MaxDelay | The maximum delay (in samples) for each delay tap | Float |