Wiki

This version (14 Sep 2022 12:58) was approved by Angu Sewa.

Click here to return to the Basic page

Voltage Controlled SPI Delay


Description

The Voltage Controlled SPI Delay cell can be used to implement off-chip delay using the SPI interface.

Targets Supported

Name ADSP-214xx ADSP-215xx/SC5xx ADAU145x/146x
——————————————————-- ——————-- ——————————-- —————————-
Voltage Controlled SPI DelayNA NA S


Pins

Input

NameTypeDescription
———————- ———————-- ———————-
Input X Audio Input Channel X
Delay X controlDelay value


Output

NameTypeDescription
———————- ———————-- ———————-
Output X Audio Output channel X

Note:

  • X - Channel Index
resources/tools-software/sigmastudiov2/modules/basic/vcspidelay.txt · Last modified: 14 Sep 2022 12:58 by Angu Sewa