Wiki

This version is outdated by a newer approved version.DiffThis version (10 Feb 2021 13:09) was approved by Sanjeeva Reddy.

This is an old revision of the document!


Click here to return to the Basic page

Value Hold


Description

The ValueHold block holds the incoming input while the control input is zero and allows the incoming input route to output while the control input is other than zero.

Targets Supported

NameADSP-214xx(Sample)ADSP-214xx(Block)ADSP-215xx/ADSP-SC5xx(Sample)ADSP-215xx/ADSP-SC5xx(Block)
ValueHold Yes YesYes Yes


Pins

Input

NameTypeDescription
HoldConditionControlHolds or allows the input signal to output
InputAudioInput channel

Output

NameTypeDescription
HeldValueAudioOutput channel


Configurable Parameters

No configurable parameters

DSP Parameters

No DSP parameters

resources/tools-software/sigmastudiov2/modules/basic/valuehold.1580809372.txt.gz · Last modified: 04 Feb 2020 10:42 by Sanjeeva Reddy