Wiki

This version (13 Sep 2022 11:34) was approved by Angu Sewa.The Previously approved version (04 Feb 2020 10:42) is available.Diff

Click here to return to the Basic page

Value Hold


Description

The ValueHold block holds the incoming input while the control input is zero and allows the incoming input route to output while the control input is other than zero.

Targets Supported

Name ADSP-214xx ADSP-215xx/SC5xx ADAU145x/146x
———————————————————— ——————-- ——————————-- —————————-
ValueHold B/S B/S S

Pins

Input

NameTypeDescription
————————————————————————————————————————
HoldConditionControlHolds or allows the input signal to output
Input XAudioInput channel X

Output

NameTypeDescription
————————————————————————————————————————
HeldValue XAudioOutput channel X

Note:

  • X - Channel Index

^GUI Parameter Name^Default Value^Range^Function Description^

———————————————————— ——— ——— ———————————————————-
NumChannels (Only for ADAU145x/146x)1 20Number of input and output channels. Change in this value requires re-compilation
resources/tools-software/sigmastudiov2/modules/basic/valuehold.txt · Last modified: 13 Sep 2022 11:34 by Angu Sewa