Wiki

The most recent version of this page is a draft.DiffThis version (10 Feb 2021 13:09) was approved by Sanjeeva Reddy.

This is an old revision of the document!


Click here to return to the Basic page

Timer With External Reset


Description

The timer block starts increment the counter value, when the control signal to Start/Reset pin is non zero and resets the counter value to zero, when the control signal to Start/Reset pin is zero. The timer continues the counter increment until it reaches the Specified value in timer input pin and its sets the flag to one upon completion.The output of the timer block is 0 or 1, indicating whether the value of timer is reached.

Targets Supported

NameADSP-214xx(Sample)ADSP-214xx(Block)ADSP-215xx/ADSP-SC5xx(Sample)ADSP-215xx/ADSP-SC5xx(Block)
TimerWithExtReset Yes YesYes Yes


Pins

Input

NameTypeDescription
StartResetControlStarts or resets the timer counter
CountValueControlSets the timer duration

Output

NameTypeDescription
TimerFlagControlIndicates the counter reached the timer value


Configurable Parameters

No configurable parameters

DSP Parameters

No DSP parameters

/srv/wiki.analog.com/data/pages/resources/tools-software/sigmastudiov2/modules/basic/timerwithextreset.txt · Last modified: 10 May 2021 11:18 by Nikhin Shetty