Wiki

The most recent version of this page is a draft.DiffThis version (10 Feb 2021 13:11) was approved by Sanjeeva Reddy.

This is an old revision of the document!


Click here to return to the Basic page

Seven Band Level Detector


Description

The Seven-Band Level Detector block calculates the input signal level, reading directly from the hardware in real-time, and displays the level graphically in seven frequency band meter displays:

  • <100Hz
  • 250Hz
  • 500Hz
  • 1kHz
  • 2.5kHz
  • 5kHz
  • >10kHz

The level detector performs the analysis only and does not modify the input signal. The signal at the output pin is identical to the input.

Use the On / Off button to enable or disable the display. The level detector will not function until the schematic design has been compiled and downloaded to the hardware and a USB communication channel is properly configured.

Targets Supported

NameADSP-214xx(Sample)ADSP-214xx(Block)ADSP-215xx/ADSP-SC5xx(Sample)ADSP-215xx/ADSP-SC5xx(Block)
Seven Band Level Detector Yes YesYes Yes


Pins

Input

Input0AudioInput Channel 0

Output

Output0ControlOutput channel 0


Configurable Parameters

No configurable parameters

DSP Parameters

No DSP Parameters

/srv/wiki.analog.com/data/pages/resources/tools-software/sigmastudiov2/modules/basic/sevenbandleveldetector.txt · Last modified: 11 May 2021 15:28 by Nikhin Shetty