Click here to return to the Basic page
The Register Read module reads any user accessible register from the DSP and gives out in the output Pin.
The Register Write module writes the value in the input pin to the DSP register address configured.
This module supports growth. Address control will be repeated for each channels when grown. And address can be specified either in hexadecimal or decimal.
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
—————————— | ——————-- | ——————————-- | —————————- |
Register Read | NA | NA | S |
Register Write | NA | NA | S |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
InputX | Control | Input Channel X (Only for RegisterWrite) |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
OutputX | Control | Output Channel X (Only for RegisterRead) |
Note:
GUI Parameter | Default Value | Range | Function Description |
---|---|---|---|
—————————————- | ———————- | ——————————-- | —————————————- |
Address X | 0xF000 | 0xF000 - 0xF890 | Register Address to be read/write |
Address Type X | Hex | Hex / Dec | Address can be specified either in hexadecimal or decimal |
Note:
Parameter Name | Description | ADSP-214xx/SC5xx/215xx | ADAU145x/146x |
---|---|---|---|
—————————————- | ———————————————————————————————————- | —————————- | —————— |
address | Register address | NA | Integer32 |