Wiki

The most recent version of this page is a draft.DiffThis version (10 Feb 2021 13:11) was approved by Sanjeeva Reddy.

This is an old revision of the document!


Click here to return to the Basic page

Real-Time Display



Description

The Real-Time Display block lets allow us read the data from the target and display it in the graph.

Usage

Click on the “Graph” icon to open the real-time display graph window. 'Start' button allows to read the data from the target for specified time of 'Time Span' and 'Stop' allows us to to stop readback from the target. 'Continous Read' allows us to read the data from the target irrespective of 'Time Span'.'Reset' resets the graph and Format allows us to specify the format of reading data.

Targets Supported

NameADSP-214xx(Sample)ADSP-214xx(Block)ADSP-215xx/ADSP-SC5xx(Sample)ADSP-215xx/ADSP-SC5xx(Block)
RMS Table Yes YesYes Yes


Pins

Input

NameTypeDescription
InputAudioInput Channel 0

Output

NameTypeDescription
OutputAudioOutput channel 0


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
Y-Max/Y-Min1 -20,000 to 20000 Displays the input signal in the specified y-axis scale
Multiplier11 to 100multiplies the input signal by this value
TimeSpan11 to 20x-axis scale- upper limit on the display

DSP Parameters

Parameter NameDescriptionADSP-214xx/SC5xx/215xx
ReadDataContains the input signal dataFloat


/srv/wiki.analog.com/data/pages/resources/tools-software/sigmastudiov2/modules/basic/realtimedisplay.txt · Last modified: 12 May 2021 07:04 by Nikhin Shetty