Wiki

This version (13 Sep 2022 11:05) was approved by Angu Sewa.

Click here to return to the Basic page

Multi-Channel Multi-Tap Delay



Description

The Multi Channel Multi Tap Delay cell provides a variable delay for each output from one of the selected input channel. Each input signal is called as channel and output is called as Tap. The amount of delay for each tap can be modified in real time by updating the current delay.

Targets Supported

Name ADSP-214xx ADSP-215xx/SC5xx ADAU145x/146x
——————————————————-- ——————-- ——————————-- —————————-
MultiChannel MultiTap DelayB B S


Pins

Input

NameTypeDescription
———————- ———————-- ———————-
Input X Audio Input Channel X


Output

NameTypeDescription
———————- ———————-- ———————-
Output X Audio Output channel X

Note:

  • X - Channel Index


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
—————————————- ———————- ———————————— —————————————-
InputSelection_OutputX_SetY Input0 Input Channels listOutput delay maximum value depends on the selected input
Delay_OutputX_SetY00 to selectedinput value current delay value
MaxDelay_InputX1010 to 2500max delay values
NumInputs120Number of input channels. Change in this value requires re-compilation
NumOutputs120Number of Output channels. Change in this value requires re-compilation

Note:

  • X - Channel Index
  • Y - Tab Index

DSP Parameters

Parameter Name Description ADSP-214xx/SC5xx/215xx ADAU145x/146x
—————————————- ——————————————————————————-- —————————————- —————————-
InputSelection_OutputXSelected input Integer32 Integer32
Delay_OutputX Current delay Integer32 Integer32
MaxDelayArray Maximum allowed Delay values Integer32 Integer32


resources/tools-software/sigmastudiov2/modules/basic/multichnlmultitapdelay.txt · Last modified: 13 Sep 2022 11:05 by Angu Sewa