This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:modules:basic:maxvaluehold [12 Nov 2019 10:03] – [Configurable Parameters] Sanjeeva Reddy | resources:tools-software:sigmastudiov2:modules:basic:maxvaluehold [07 May 2021 13:28] – [Targets Supported] Nikhin Shetty | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources/ | [[resources/ | ||
====== Max Value Hold ====== | ====== Max Value Hold ====== | ||
+ | \\ | ||
+ | {{: | ||
===== Description ===== | ===== Description ===== | ||
The MaxValueHold block monitors one (or more) input(s) and routes the max value of the input to the output. This block held's the max value while the control input is 1 and reset the max value while the control input is 0. | The MaxValueHold block monitors one (or more) input(s) and routes the max value of the input to the output. This block held's the max value while the control input is 1 and reset the max value while the control input is 0. | ||
+ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/ |
- | |MaxValueHold| Yes | Yes|Yes| Yes| | + | | ------------------------------------------------------------ |
+ | |MaxValueHold| B/S | B/S | B/S | | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | |------------------------------|------------------------------------------------------------|------------------------------| | ||
|Reset|Control|Resets the maximum value| | |Reset|Control|Resets the maximum value| | ||
- | |Input0|Audio|Input channel | + | |Input<fc # |
+ | Note: | ||
+ | * <fc # | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | |Output0|Audio|Output channel | + | |------------------------------|------------------------------------------------------------|------------------------------| |
+ | |Output | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | |------------------------------|---------------------------|----------------------------|----------------------------------------------------------| | ||
|NumChannels|1| 20|Number of input and output channels. Change in this value requires re-compilation| | |NumChannels|1| 20|Number of input and output channels. Change in this value requires re-compilation| | ||
- | ===== DSP Parameters ===== | + | \\ |
- | No DSP parameters | + |