This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudiov2:modules:basic:maxvaluehold [07 May 2021 13:28] – [Targets Supported] Nikhin Shetty | resources:tools-software:sigmastudiov2:modules:basic:maxvaluehold [13 Sep 2022 11:33] (current) – Updates Image Angu Sewa | ||
---|---|---|---|
Line 2: | Line 2: | ||
====== Max Value Hold ====== | ====== Max Value Hold ====== | ||
\\ | \\ | ||
- | {{: | + | {{: |
===== Description ===== | ===== Description ===== | ||
The MaxValueHold block monitors one (or more) input(s) and routes the max value of the input to the output. This block held's the max value while the control input is 1 and reset the max value while the control input is 0. | The MaxValueHold block monitors one (or more) input(s) and routes the max value of the input to the output. This block held's the max value while the control input is 1 and reset the max value while the control input is 0. |