This is an old revision of the document!
Click here to return to the Basic page
The feedback algorithm generates a delay in the signal path and reroutes signal to an input occurring earlier in the path. Note that this block must be used if feedback is required in your design.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
Feedback | Yes | Yes | Yes | Yes |
Name | Type | Descrption |
---|---|---|
Input0 | Audio | Input Channel 0 |
Name | Type | Descrption |
---|---|---|
Output0 | Control | Output channel 0 |
No configurable parameters
No DSP Parameters