Wiki

This version (14 Sep 2022 12:54) was approved by Angu Sewa.

Click here to return to the Basic page

External SPI Delay


Description

The External SPI Delay cell can be used to implement off-chip delay using the SPI interface.

Targets Supported

Name ADSP-214xx ADSP-215xx/SC5xx ADAU145x/146x
——————————————————-- ——————-- ——————————-- —————————-
Fractional DelayNA NA S


Pins

Input

NameTypeDescription
———————- ———————-- ———————-
Input X Audio Input Channel X


Output

NameTypeDescription
———————- ———————-- ———————-
Output X Audio Output channel X

Note:

  • X - Channel Index
resources/tools-software/sigmastudiov2/modules/basic/extspidelay.txt · Last modified: 14 Sep 2022 12:54 by Angu Sewa