Click here to return to the Basic page
The clipping detection module can be used to identify whether there is a clipping in a particular wave form. It indicates the signal reaching the onset of its maximum permitted peak-to-peak voltage value before an overload is occurring. This will help in preventing severe, audible distortion to be generated through the audio signal chain.
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
—————————— | ——————-- | ——————————-- | —————————- |
Clipping Detection | NA | B | NA |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
Input0 | Audio | Input channel0 |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
Output0 | Audio | Output channel0 |
ClippingFlag | Control | Clipping detection flag |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
—————————————- | ———————- | —————— | —————————————- |
Enable | False | True / False | Enable or disable the clipping detection |
Delay | 64 | 8 to 1024 | Scales the delay factor |
FixedAddress | False | True / False | Enable or disable the Fixed Address mode |
OutBlockSizeFactor | 2 | 2 to 10 | Scales the Block size out factor |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx | ADAU145x/146x |
---|---|---|---|
—————————————- | ——————————————————————————-- | —————————————- | —————————- |
Enable | zero or one depends on the state | Integer32 | NA |
Delay | Delay Factor | Integer32 | NA |