This is an old revision of the document!
Click here to return to the Basic page
The AbsMaxValueHold block monitors one (or more) input(s) and routes the absolute max value of the input to the output. This block helds the absolute max value while the control input is 1 and reset the absolute max value while the control input is 0.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
AbsMaxValueHold | Yes | Yes | Yes | Yes |
Name | Type | Description |
---|---|---|
Reset | Control | Resets the absolute maximum value |
Input0 | Audio | Input channel 0 |
Name | Type | Description |
---|---|---|
Output0 | Audio | Output channel 0 |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
NumChannels | 1 | 20 | Number of input and output channels. Change in this value requires re-compilation |
No DSP parameters