This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:squaresummation [04 Feb 2020 07:36] Sanjeeva Reddy Added an image |
resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:squaresummation [06 May 2021 11:37] Krithika Manchale |
||
---|---|---|---|
Line 10: | Line 10: | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ADSP-SC5xx(Sample)^ADSP-215xx/ADSP-SC5xx(Block)^ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/SC5xx ^ ADAU145x/146x ^ |
- | |Square Summation | No | Yes|No| Yes| | + | | ------------------------------------------- | ---------------------------- | ----------------------------- | ---------------------------- | |
+ | | Square Summation| B | B | NA | | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ------------------------------------ | ------------------------- | ---------------------------------------- | | ||
|Reset|Control|Resets the summation result| | |Reset|Control|Resets the summation result| | ||
|Input0|Audio|Input channel 10| | |Input0|Audio|Input channel 10| | ||
Line 21: | Line 23: | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ------------------------------------ | ------------------------ | ---------------------------------------- | | ||
|Output0|Audio|Output channel 0| | |Output0|Audio|Output channel 0| | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
^GUI Parameter Name^Default Value^Range^Function Description^ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
- | |NumChannels|2|20|Number of input and output channels. Change in this value requires re-compilation| | + | | ---------------------------------------- | ---------------------- | --------------------------| ------------------------------------------------------------------- | |
+ | |NumChannels|2|20|Number of in/out channels. Change in this value requires re-compilation| | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
No DSP parameters | No DSP parameters | ||