Wiki

This version (18 May 2021 08:51) was approved by John Joseph.The Previously approved version (04 Feb 2020 07:36) is available.Diff

Click here to return to the Arithmetic and Logic page

Square Summation


Description

The Square Summation block adds the square of the input to the sum of previous square of inputs and outputs the result of sum.

Usage

The Reset pin is available to reset the summation result. Other than the zero to reset pin, resets the summation value.

Targets Supported

Name ADSP-214xx ADSP-215xx/SC5xx ADAU145x/146x
——————————————- —————————- —————————-- —————————-
Square Summation B B NA

Pins

Input

NameTypeDescription
———————————— ————————- —————————————-
ResetControlResets the summation result
Input0AudioInput channel 10

Output

NameTypeDescription
———————————— ———————— —————————————-
Output0AudioOutput channel 0

Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
—————————————- ———————- ————————-- ——————————————————————-
NumChannels220Number of in/out channels. Change in this value requires re-compilation

DSP Parameters

No DSP parameters

resources/tools-software/sigmastudiov2/modules/arithmeticandlogic/squaresummation.txt · Last modified: 06 May 2021 11:37 by Krithika Manchale