Wiki

This version is outdated by a newer approved version.DiffThis version (18 May 2021 08:50) was approved by John Joseph.The Previously approved version (04 Feb 2020 07:31) is available.Diff

This is an old revision of the document!


Click here to return to the Arithmetic and Logic page

Signal Add


Description

The Signal Add block adds the inputs together and no other modification of the signal is done. Care must be taken to avoid clipping.

Variants

  1. Signal Add
  2. Complex Signal Add
  3. Scalar Add


Targets Supported

Name ADSP-214xx ADSP-215xx/SC5xx ADAU145x/146x
—————————— ——————-- ——————————-- —————————-
Signal Add B/S B/S S
Complex Signal Add NA NA B
Scalar Add NA NA B


Pins

Input

NameTypeDescription
————————————— —————————- —————————————
Input0AudioInput channel 0
Input1AudioInput channel 1

Output

NameTypeDescription
————————————-- —————————- —————————————-
SumAudioOutput channel

Configurable Parameters

GUI Parameter NameDefault Value RangeFunction Description
—————————— ——————————- ————————————-- ——————————————————-
NumChannels220Number of input channels.Change in this value require re-compilation

DSP Parameters

NO DSP Parameters

resources/tools-software/sigmastudiov2/modules/arithmeticandlogic/signaladd.1620294737.txt.gz · Last modified: 06 May 2021 11:52 by Krithika Manchale