This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:rmswithtc [27 Feb 2020 05:12] Krithika Manchale [DSP Parameters] |
resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:rmswithtc [07 May 2021 07:22] Krithika Manchale [DSP Parameters] |
||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources/tools-software/sigmastudiov2/modules/arithmeticandlogic|Click here to return to the Arithmetic and Logic page]] | [[resources/tools-software/sigmastudiov2/modules/arithmeticandlogic|Click here to return to the Arithmetic and Logic page]] | ||
- | ====== RMSWithTC ====== | + | ====== RMS With TC ====== |
\\ | \\ | ||
{{:resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:rmswtc.png}} | {{:resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:rmswtc.png}} | ||
Line 7: | Line 7: | ||
\\ | \\ | ||
===== Targets Supported ===== | ===== Targets Supported ===== | ||
- | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ADSP-SC5xx(Sample)^ADSP-215xx/ADSP-SC5xx(Block)^ | + | ^ Name ^ ADSP-214xx ^ ADSP-215xx/SC5xx ^ ADAU145x/146x ^ |
- | |RMSWithTC | Yes | Yes|Yes| Yes| | + | | ------------------------------ | -------------------- | -------------------------------- | ---------------------------- | |
+ | | RMSWithTC | S/B | S/B | NA | | ||
\\ | \\ | ||
===== Pins ===== | ===== Pins ===== | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ------------------------------------ | ------------------------------ | ---------------------------------------- | | ||
|Input0|Audio|Input channel 10| | |Input0|Audio|Input channel 10| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
+ | | ------------------------------------ | ------------------------------ | ---------------------------------------- | | ||
|Output0|Audio|Output channel 0| | |Output0|Audio|Output channel 0| | ||
===== Configurable Parameters ===== | ===== Configurable Parameters ===== | ||
- | ^GUI Parameter Name^Default Value^Range^Function Description^ | + | ^GUI Parameter Name ^Default Value ^Range ^Function Description^ |
- | |TimeConstant|121|1-8686|Determines how rapidly the RMS value is to be computed with any change in the input level | | + | | ---------------------------------------- | ---------------------------- | ------------------------------------- |---------------------------------------------------------------- | |
- | |IsDBps|False|Truie/False|Control value in dB/s or ms| | + | |TimeConstant|121 |1-8686 |Determines how rapidly the RMS value is to be computed with any change in the input level | |
- | |NumChannels|2|20|Number of input and Output channels. Change in this value requires re-compilation| | + | |IsDBps|False |True/False |Control value in dB/s or ms| |
+ | |NumChannels|2 |20 |Number of input and Output channels. Change in this value requires re-compilation| | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
^Parameter Name^Description^ADSP-214xx/215xx/SC5xx^ | ^Parameter Name^Description^ADSP-214xx/215xx/SC5xx^ | ||
- | |TimeConstant| TC for RMS value compute with change in input level| Float| | + | |-------------------------------- |------------------------------------------------------------------ |-------------------------------------------| |
+ | |TimeConstant| TC for RMS value with change in input| Float| | ||
===== DSP Parameter Computation ===== | ===== DSP Parameter Computation ===== |