Click here to return to the Arithmetic and Logic page
Polynomial
Description
The Polynomial block computes the polynomial equation of (N - 1)th order.Where N specifies in the text field.
Usage
Enter the order of the equation in the text field and to open the table editor to enter the coefficients, click on the table button.
if N = 5, This block computes the polynomial equation of 4th order.The table editor contains 5 coefficients and those are in the order of a0,a1,a2,a3, and a4 respectively.
Variants
1. SinglePrecision
2. ExtendedPrecision
Targets Supported
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
—————————— | ——————-- | ——————————-- | —————————- |
SinglePrecision | B/S | B/S | NA |
ExtendedPrecision | B/S | B/S | NA |
Pins
Name | Type | Description |
————————————— | —————————- | ————————————— |
Input | Audio | Input channel |
Output
Name | Type | Description |
————————————— | —————————- | ————————————— |
Output | Audio | Output channel |
Configurable Parameters
GUI Parameter Name | Default Value | Range | Function Description |
—————————————— | ————————-- | ————————— | ————————————————————————-- |
NumofTableValues | 2 | 2 to 50000 | N -1 order of the equation |
TableValues | 1 and 2 | coefficients values a0,a1 |
PrecsisonType | SinglePrecision | Single/Extended | Changes the algorithm type and requires re-compilation |
DSP Parameters
Parameter Name | Description | ADSP-214xx/SC5xx/215xx | |
———————————— | ———————————————————- | ———————————————- | ————————————— |
NumofTableValues | N -1 order of the equation | Float | |
TableValues | coeffcients values a0,a1 | Float | |