This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:oneshotraise [06 May 2021 14:33] – [DSP Parameters] Krithika Manchale | resources:tools-software:sigmastudiov2:modules:arithmeticandlogic:oneshotraise [14 Sep 2022 13:42] (current) – [Description] Angu Sewa | ||
---|---|---|---|
Line 6: | Line 6: | ||
{{: | {{: | ||
===== Description ===== | ===== Description ===== | ||
- | The One Shot Rise block outputs a trigger signal based upon the rising edge of the input signal. At the first non-zero rising edge of the input signal, the output signal will go high and remain high.For One Shot Raise Reset block the output signal will remain high until a non-zero input signal is seen on the rest pin. The reset pin clears the output back to zero and will maintain the output at zero while the signal on the reset pin is non-zero. | + | The One Shot Rise block outputs a trigger signal based upon the rising edge of the input signal. At the first non-zero rising edge of the input signal, the output signal will go high and remain high. For One Shot Raise Reset block the output signal will remain high until a non-zero input signal is seen on the rest pin. The reset pin clears the output back to zero and will maintain the output at zero while the signal on the reset pin is non-zero. |
\\ | \\ | ||
\\ | \\ | ||
Line 24: | Line 24: | ||
==== Input ==== | ==== Input ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | | --------------------------------------- | ---------------------------- | --------------------------------------- | | + | | --------------------------------------- | ---------------------------- | ------------------------------------------------------- | |
|Input|Audio|Input signal that is monitored for the first falling edge| | |Input|Audio|Input signal that is monitored for the first falling edge| | ||
|Reset|Control|Resets the output trigger signal back to zero(only for OneShotRiseReset)| | |Reset|Control|Resets the output trigger signal back to zero(only for OneShotRiseReset)| | ||
==== Output ==== | ==== Output ==== | ||
^Name^Type^Description^ | ^Name^Type^Description^ | ||
- | | --------------------------------------- | ---------------------------- | --------------------------------------- | | + | | --------------------------------------- | ---------------------------- | -------------------------------------------------------- | |
|Output|Control|Sets bit position of the output “1” flag| | |Output|Control|Sets bit position of the output “1” flag| | ||
\\ | \\ | ||
Line 38: | Line 38: | ||
\\ | \\ | ||
===== DSP Parameters ===== | ===== DSP Parameters ===== | ||
- | ^Parameter Name^Description^ADSP-214xx/ | + | ^Parameter Name^Description^ADSP-214xx/ |
- | | ------------------------------------ | -------------------------------------------------------------------------- | + | | ------------------------------------ | ----------------------------------------------------------------- | ---------------------------------------- | --------------------------------------- | |
|BitVal| Compute & set the bit position value| FixInt32| FixInt32| | |BitVal| Compute & set the bit position value| FixInt32| FixInt32| | ||
\\ | \\ | ||