Wiki

This version (18 May 2021 08:56) was approved by Nikhin Shetty.

Click here to return to the Arithmetic and Logic page

One Shot Rise



Description

The One Shot Rise block outputs a trigger signal based upon the rising edge of the input signal. At the first non-zero rising edge of the input signal, the output signal will go high and remain high.For One Shot Raise Reset block the output signal will remain high until a non-zero input signal is seen on the rest pin. The reset pin clears the output back to zero and will maintain the output at zero while the signal on the reset pin is non-zero.

If the input signal starts high, the output signal will start and remain high.

Variants

  1. One Shot Rise
  2. One Shot Rise Reset


Targets Supported

Name ADSP-214xx ADSP-215xx/SC5xx ADAU145x/146x
—————————— ————————- ——————————-- —————————-
OneShotRise B/S B/S S
OneShotRiseReset B/S B/S S


Pins

Input

NameTypeDescription
————————————— —————————- ——————————————————-
InputAudioInput signal that is monitored for the first falling edge
ResetControlResets the output trigger signal back to zero(only for OneShotRiseReset)

Output

NameTypeDescription
————————————— —————————- ——————————————————--
OutputControlSets bit position of the output “1” flag


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
—————————————— ————————-- ————————— ————————————————————————--
Selected BitBit:0Bit:30Sets bit position of Output'1' Flag.


DSP Parameters

Parameter NameDescriptionADSP-214xx/215xx/SC5xxADAU145x/6x
———————————— —————————————————————-- —————————————- —————————————
BitVal Compute & set the bit position value FixInt32 FixInt32


resources/tools-software/sigmastudiov2/modules/arithmeticandlogic/oneshotraise.txt · Last modified: 07 May 2021 07:48 by Krithika Manchale