This is an old revision of the document!
Click here to return to the AdvancedDSP page
The Up sampling module is mainly used to get the input samples to a higher sampling rates after processing the audio at lower sampling rates.For example the bass of the audio can be processed at lower sampling rates and then taken to the higher sampling rates.
This module takes the upsample factor from the GUI parameters and upsample the input accordingly.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
UpSampler | No | No | No | Yes |
Name | Type | Description |
---|---|---|
Input | Audio | Input channel |
Name | Type | Description |
---|---|---|
Output | Audio | Up sampled output |
GUI Parameter Name | Default | Range | Function Description |
---|---|---|---|
Factor | 2 | 2,4,8,16,32 | The factor at with the input sample rate will be multiplied |
DisableFilter | False | True/False | Enabled/Disabled the filter. If enabled, filter will be applied after upsampling the signal |
Name | Description | ADSP-214xx/215xx/SC5xx |
---|---|---|
Factor | The factor at with the input sample rate will be multiplied | Float |
NFilterTaps | Number of antialiasing filter coefficients | Float |
FIRCoeffs | coefficients | Float |
NFilterTaps = Factor >= 16 ? 97:49