Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:sigmastudiov2:modules:adialgorithms:loudnesswithfilter [26 Feb 2020 08:27]
Sreesha Y M [DSP Parameter Computation]
resources:tools-software:sigmastudiov2:modules:adialgorithms:loudnesswithfilter [11 May 2021 09:46]
John Joseph Formatting updated
Line 1: Line 1:
 [[resources/​tools-software/​sigmastudiov2/​modules/​adialgorithms|Click here to return to the ADI Algorithms page]] [[resources/​tools-software/​sigmastudiov2/​modules/​adialgorithms|Click here to return to the ADI Algorithms page]]
 ====== Loudness With Filter ====== ====== Loudness With Filter ======
-\\ +{{:​resources:​tools-software:​sigmastudiov2:​modules:​adialgorithms:​loudnesswfilter.png?​nolink&​150}}
-{{:​resources:​tools-software:​sigmastudiov2:​modules:​adialgorithms:​loudnesswfilter.png?​200}}+
 ===== Description ===== ===== Description =====
 \\ \\
Line 13: Line 12:
   * First-Order High Shelf   * First-Order High Shelf
   * Peaking ​   * Peaking ​
 +\\
 ===== Usage ===== ===== Usage =====
- 
 To access the filter click on the icon button and icon button image will change to reflect the selected filter type To access the filter click on the icon button and icon button image will change to reflect the selected filter type
 +\\ 
 +\\
 ===== Targets Supported ===== ===== Targets Supported =====
-^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/​ADSP-SC5xx(Sample)^ADSP-215xx/ADSP-SC5xx(Block)+^ Name            ^ ADSP-214xx ^ ADSP-215xx/​SC5xx ^ ADAU145x/146x ^ 
-|Loudness With Filter| ​No | No|NoYes|+| ------------------------------ | -------------------- | -------------------------------- | ---------------------------- | 
 +| Loudness With Filter ​  ​B          ​B                ​NA              ​|
 \\ \\
 ===== Pins ===== ===== Pins =====
 ==== Input ==== ==== Input ====
 ^Name^Type^Description^ ^Name^Type^Description^
 +| ---------------------- | -------------- | ---------------------- |
 |ControlInput|Control|External volume controls the loudness applied to the filtered input signal| |ControlInput|Control|External volume controls the loudness applied to the filtered input signal|
 |Input0|Audio|Input Channel0| |Input0|Audio|Input Channel0|
 ==== Output ==== ==== Output ====
 +^Name^Type^Description^
 +| ---------------------- | -------------- | ---------------------- |
 |Output0|Audio|Output channel0| |Output0|Audio|Output channel0|
 +\\
 ===== Configurable Parameters ===== ===== Configurable Parameters =====
 ^GUI Parameter Name^Default Value^Range^Function Description^ ^GUI Parameter Name^Default Value^Range^Function Description^
 +| ---------------------------------------- | ---------------------- | ------------------ | ---------------------------------------- |
 |Boost|0dB|-20 to 20 dB| Set the boost value for a particular filter curve| |Boost|0dB|-20 to 20 dB| Set the boost value for a particular filter curve|
 |Frequency|1000Hz|20 to 20000Hz|The cutoff frequency of the filter| |Frequency|1000Hz|20 to 20000Hz|The cutoff frequency of the filter|
Line 38: Line 44:
 |FilterType|Low Shelf Filter| - | Selects the desired filter type| |FilterType|Low Shelf Filter| - | Selects the desired filter type|
 |NumChannels|1|20|Number of input and output channels. Change in this value requires re-compilation| |NumChannels|1|20|Number of input and output channels. Change in this value requires re-compilation|
 +\\
 ===== DSP Parameters ===== ===== DSP Parameters =====
 ^Parameter Name^Description^ADSP-214xx/​SC5xx/​215xx^ ^Parameter Name^Description^ADSP-214xx/​SC5xx/​215xx^
 +| ---------------------------------------- | ------------------------------------------------------------ | ---------------------------------------- |
 |A1|Coefficient A1    |Float| |A1|Coefficient A1    |Float|
 |A2|Coefficient A2    |Float| |A2|Coefficient A2    |Float|
Line 46: Line 54:
 |B2|Coefficient B2    |Float| |B2|Coefficient B2    |Float|
  
-===== DSP Parameter Computation ===== 
resources/tools-software/sigmastudiov2/modules/adialgorithms/loudnesswithfilter.txt · Last modified: 11 May 2021 09:46 by John Joseph