Click here to return to the ADI Algorithms page
The Dynamic Enhancement block provides variable bass enhancement as a function of input-signal level. Lower levels require more bass than higher levels. The filter dynamically adjusts the amount of bass enhancement depending on the volume of the input signal, by using a variable-Q filter.
A fixed enhancement is applied to input levels below the threshold while a dynamic gain is applied to input levels above the threshold.
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
---|---|---|---|
———————————————— | ——————-- | ——————————-- | —————————- |
Dynamic Enhancement (Mono) | B/S | B/S | NA |
Dynamic Enhancement (Stereo) | B/S | B/S | NA |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
Input0 | Audio | Input channel0 |
Input1 | Audio | Input Channel1 (only for stereo) |
Name | Type | Description |
---|---|---|
———————- | ————-- | ———————- |
Output0 | Audio | Output channel0 |
Output1 | Audio | Output channel1 (only for stereo) |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
—————————————- | ———————- | —————— | —————————————- |
TimeConstant | 100 ms | 0 to 500ms | This controls the RMS time constant for the detector. Changing the attack and release rates |
CompThreshold | -5 db | -24 to 20 dB | Threshold of the detector.Any signal coming into the detector below the threshold level will not influence the boost calculation. it receives a fixed enhancement. |
CompressorRatio | 3 | 1 to 15 | It is dynamic boost ratio.Controls the rate at which the bass boost changes from the low to the high threshold. |
BoostFrequency | 6 Hz | 0 to 16 Hz | Controls the maximum dynamic enhancement gain applied to the algorithm. |
BassFrequency | 60 hz | 20 to 300 Hz | Cut off frequency for the boosting filter. |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx |
---|---|---|
—————————————- | —————————————————————————————— | —————————————- |
CompThreshold | Threshold of the detector | Float |
TimeConstant | Rms time constant for the detector for change in input signal level | Float |
BoostFrequency | maximum dynamic enhancement gain applied to the algorithm | Float |
BassFrequency | Cut off frequency for the boosting filter | Float |