Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:sigmastudiov2:gettingstarted:swsetup [20 Sep 2022 14:50] – Removes eval from the installer name Ashwin PSresources:tools-software:sigmastudiov2:gettingstarted:swsetup [26 Sep 2023 13:28] (current) John Joseph
Line 8: Line 8:
   - [[adi>en/design-center/evaluation-hardware-and-software/software/adswt-cces.html|CrossCore Embedded Studio]] - SigmaStudio uses the tools that are included with CrossCore Embedded Studio. Install CrossCore Embedded Studio, if it is not already installed on the SigmaStudio+ Host PC.    - [[adi>en/design-center/evaluation-hardware-and-software/software/adswt-cces.html|CrossCore Embedded Studio]] - SigmaStudio uses the tools that are included with CrossCore Embedded Studio. Install CrossCore Embedded Studio, if it is not already installed on the SigmaStudio+ Host PC. 
   - [[http://download.analog.com/tools/EZBoards/SC5xx/Releases/Release_2.0.2/ADI_ADSP-SC5xx_EZ-KIT_Lite-Rel2.0.2.exe|ADSP-SC5xx Board Support package]]   - [[http://download.analog.com/tools/EZBoards/SC5xx/Releases/Release_2.0.2/ADI_ADSP-SC5xx_EZ-KIT_Lite-Rel2.0.2.exe|ADSP-SC5xx Board Support package]]
-  - Install SigmaStudio+ version 2.0.0 ADI_SigmaStudioPlus-Rel2.0.0.exe+  - Install the latest version of [[adi>en/design-center/evaluation-hardware-and-software/software/sigmastudio-plus.html#software-overview|SigmaStudio+]].
  
  
-<note tip>Note that if more than one version of the CrossCore Embedded Studio tool-chain is detected, the Processor Settings of ADSP-214xx/ADSP-215xx/ADSP-SC5xx allows for tool-chain selection. +<note tip>If multiple versions of the CrossCore Embedded Studio are installed, one of the tool-chain versions can be selected in the processor settings page of ADSP-214xx/ADSP-215xx/ADSP-SC5xx”. “ADSP-214xx/ADSP-215xx/ADSP-SC5xx” processor settings page can be launched from the Project Window.</note>
-</note>+
  
 ===== ADAU145x/ADAU146x ===== ===== ADAU145x/ADAU146x =====
  
-  - Install SigmaStudio+ version 2.0.0 ADI_SigmaStudioPlus-Rel2.0.0.exe+  - Install the latest version of [[adi>en/design-center/evaluation-hardware-and-software/software/sigmastudio-plus.html#software-overview|SigmaStudio+]].
resources/tools-software/sigmastudiov2/gettingstarted/swsetup.txt · Last modified: 26 Sep 2023 13:28 by John Joseph