This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:sigmastudiov2:gettingstarted:executeexampleproject [02 Jul 2020 15:56] – details updated John Joseph | resources:tools-software:sigmastudiov2:gettingstarted:executeexampleproject [05 May 2021 14:03] – Details updated for SigmaDSP John Joseph | ||
---|---|---|---|
Line 1: | Line 1: | ||
[[resources: | [[resources: | ||
- | =====Execute Example Project===== | + | ======Execute Example Project====== |
- | ==== Download Example Projects ==== | + | ===== Download Example Projects |
Example projects can be downloaded from [[resources: | Example projects can be downloaded from [[resources: | ||
\\ | \\ | ||
\\ | \\ | ||
- | ==== Load and Execute Target Application ==== | + | ===== Load and Execute Target Application |
- | \\ | + | |
Target application has to loaded on to the evaluation platform before executing the example applications on ADSP-214xx, ADSP-215xx and ADSP-SC5xx platforms. There are two options to load the application on the target platform. | Target application has to loaded on to the evaluation platform before executing the example applications on ADSP-214xx, ADSP-215xx and ADSP-SC5xx platforms. There are two options to load the application on the target platform. | ||
\\ | \\ | ||
Line 22: | Line 21: | ||
\\ | \\ | ||
\\ | \\ | ||
- | ====Download and Tune using SigmaStudio+==== | + | =====Download and Tune using SigmaStudio+===== |
- Double click on the downloaded project file to open it in SigmaStudio+. | - Double click on the downloaded project file to open it in SigmaStudio+. | ||
- Click ' | - Click ' | ||
- Navigate to the schematic canvas by clicking on the schematic from the Schematic panel | - Navigate to the schematic canvas by clicking on the schematic from the Schematic panel | ||
- Change the graphical controls | - Change the graphical controls | ||
- | \\ | ||
\\ | \\ | ||
Refer to [[resources: | Refer to [[resources: | ||
Line 33: | Line 31: | ||
Refer to [[resources: | Refer to [[resources: | ||
- | Refer to [[resources: | + | Refer to [[resources: |
+ | \\ | ||
+ | < | ||