ADSP-SC573 Board Connections
ADSP-21573 Board Connections
The board settings for running SigmaStudio on ADSP-SC573 EZ-BOARD, using the Default Application is given in the below tables.
SW1 | Position 0 |
SW6 | ON, OFF, ON, OFF, ON, OFF |
SW7 | ON, OFF, ON, OFF, OFF, OFF |
SW8 | OFF, OFF |
Switch Settings for ADSP-SC573 EZ-BOARD
Jumper | Setting |
---|---|
JP1 | Not connected |
JP2 | Not connected |
JP3 | Not connected |
JP4 | Not connected |
Jumper Settings for ADSP-SC573 EZ-BOARD
Port | Setting |
---|---|
P2 | Connected with SigmaStudio USBi |
P17 | Connected |
P18 | Connected |
P20 | Connected |
P21 | Connected |
P24 | Connected |
P25 | All pairs of jumpers are connected |
Port Settings for ADSP-SC573 EZ-BOARD