Wiki

This version (10 Feb 2021 11:50) was approved by Sreesha Y M.

Click here to return back

Schematic Window



The schematic window contains the link to all the schematics present in the project. Instead of iterating through the project window to find the different schematics, this window acts as a shortcut having links to all the schematics present. The schematic window is docked horizontally right and vertically at the center of the screen by default. The visibility of the window can be changed based on users requirement from the top menu.

There are two icons depicted to the left of the schematic name. The first icon opens the settings page of the schematic and the second icon opens the canvas on which the schematic can be designed.

resources/tools-software/sigmastudiov2/developmentenvironment/schematicwindow/schematic_window.txt · Last modified: 06 Jul 2020 08:00 by Sreesha Y M