Wiki

This version (10 Feb 2021 11:50) was approved by Sreesha Y M.

Click here to return back

Properties Window



The properties window displays all the details related to any element that is present on the canvas. The properties window is docked at the bottom right by default when SigmaStudio+ is launched. When a particular element on the canvas is selected, all the details of the module which include name, uid, version, processing type, blocksize, sampling rate, number of channels or stages if any and bypass options are displayed. The figure above depicts the details of dynamic bass boost mono module instance.

The option of bypassing the module, excluding the export and changing the precision type, number of channels, stages can be done through the properties window. These options are also available in the context menu which appears upon right click on the module.

resources/tools-software/sigmastudiov2/developmentenvironment/propertieswindow/properties_window.txt · Last modified: 15 Jul 2020 13:52 by Raghavendra Habbu