Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:tools-software:sigmastudiov2:developmentenvironment:outputwindow:output_window [07 Jul 2020 07:07] – created Sreesha Y M | resources:tools-software:sigmastudiov2:developmentenvironment:outputwindow:output_window [15 Mar 2024 14:14] (current) – spelling Arpit Arora |
---|
[[resources/tools-software/sigmastudiov2/developmentenvironment|Click here to return back]] | [[resources/tools-software/sigmastudiov2/developmentenvironment|Click here to return back]] |
\\ | \\ |
| |
====== Output Window ====== | ====== Output Window ====== |
{{:resources:tools-software:sigmastudiov2:developmentenvironment:outputwindow:outputwindow.png?1000|}} | {{:resources:tools-software:sigmastudiov2:developmentenvironment:outputwindow:outputwindow.png?nolink|}} |
\\ | \\ |
\\ | \\ |
The Output window is a quick way to view the files generated upon linking, compiling, and other actions in the schematic workspace. By default this window is docked at the bottom of the tool. The output window displays all the error messages which would have occurred due to different user actions. During linking, compilation and target download if there are are any issues, which include linking errors due to incomplete schematic, compilation issues, dxe not loaded or dxe not matching with expected target etc, all these are displayed in the output window. | All the output log messages, including error messages, generated upon project linking, compiling, and other actions performed on the project are displayed on the Output Window. By default, this window is docked at the bottom of the application. SigmaStudio+ navigates and highlights the source of error when user clicks on any error message displayed on the output window. |
\\ | \\ |
The top right corner of the output window has a button which is used for clearing the contents of the output window, which will be enabled only when the output window is not empty. | \\ |
| Following additional features are provided on the Output Window: |
| - **Clear Entries** - Clears the contents of the output window, which will be enabled only when the output window is not empty. |
| - **Copy To Clipboard** - Copies the entire output window content to clipboard. |
| - **Enable Logging** - - Enables logging functionality of the output window. Once enabled, every entry in the output window will be written to the file “OutputWindowLog_<DataAndTime>.txt” in “Log/OutputWindow” folder relative to SigmaStudio+ application. Every output window entry is logged to the file if the “Enable Logging” is checked. Once disabled, the output window stops logging messages to this file. On re-enabling the logging, a new output window log file is generated by SigmaStudio+, and messages displayed after enabling logging are further written to this new file. |