Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:sigmastudiov2:developmentenvironment:outputwindow:output_window [01 Jul 2020 10:55] – created Sreesha Y Mresources:tools-software:sigmastudiov2:developmentenvironment:outputwindow:output_window [15 Mar 2024 14:14] (current) – spelling Arpit Arora
Line 1: Line 1:
 [[resources/tools-software/sigmastudiov2/developmentenvironment|Click here to return back]] [[resources/tools-software/sigmastudiov2/developmentenvironment|Click here to return back]]
 \\ \\
- 
 ====== Output Window ====== ====== Output Window ======
-{{:resources:tools-software:sigmastudiov2:developmentenvironment:outputwindow:outputwindow.png?1000|}}+{{:resources:tools-software:sigmastudiov2:developmentenvironment:outputwindow:outputwindow.png?nolink|}}
 \\ \\
 \\ \\
-The Output window is a quick way to view the files generated upon linking, compiling, and other actions in the Schematic workspace. By default this window is docked at the bottom of the toolThe output window displays all the error messages which would have occurred due to different user actionsDuring linkingcompilation and target download if there are are any issues like linking errors due to incomplete schematic, compilation issues, dxe not loaded or dxe not matching with expected target etc are all displayed in the output window.+All the output log messages, including error messages, generated upon project linking, compiling, and other actions performed on the project are displayed on the Output Window. By defaultthis window is docked at the bottom of the applicationSigmaStudio+ navigates and highlights the source of error when user clicks on any error message displayed on the output window
 +\\ 
 +\\ 
 +Following additional features are provided on the Output Window: 
 +    - **Clear Entries** - Clears the contents of the output window, which will be enabled only when the output window is not empty. 
 +    - **Copy To Clipboard** - Copies the entire output window content to clipboard. 
 +    - **Enable Logging** - - Enables logging functionality of the output window. Once enabledevery entry in the output window will be written to the file “OutputWindowLog_<DataAndTime>.txt” in “Log/OutputWindow” folder relative to SigmaStudio+ application. Every output window entry is logged to the file if the “Enable Logging” is checked. Once disabled, the output window stops logging messages to this file. On re-enabling the logging, a new output window log file is generated by SigmaStudio+, and messages displayed after enabling logging are further written to this new file
resources/tools-software/sigmastudiov2/developmentenvironment/outputwindow/output_window.1593593728.txt.gz · Last modified: 01 Jul 2020 10:55 by Sreesha Y M