Click here to return back
The application toolbars provide buttons for common commands. The toolbar on top provides buttons with different functionalities which actually act as short-cut. These functionalities can also be chosen from the menu. Some of the options available through the toolbar include new project, open project, save project, close project, undo, redo, zoom in , zoom out, link, link compile, link compile download, clean link compile download and presets.
The individual menu options are described in brief below.
New Project - Create a new Project
Open Project - Open an Existing Project
Recent Projects- List of projects opened recently
Close Project - Close the current open projects
Save - Save the current project
Save As - Save the current project in a desired location
Print Canvas - Print the canvas area consisting of modules and connectors
Export Canvas - Export the canvas area as an image
Exit - Exit Sigma Studio+
Undo - Undo the recent operation performed
Redo - Redo the most recent undone operation
Cut - Cut the selected item or group of items
Copy - Copy the selected item or group of items
Paste - Paste the copied/cut items
Zoom-In- Magnify the canvas area
Zoom-Out - Shrink the canvas area
Zoom to Fit - Adjust the canvas area to the screen such that the entire schematic is visible on the screen
Reset Layout - Reset the layout
Activate Design Layout - Activate Design Layout
Activate Tune Layout - Activate Tune Layout
Enable/Disable Window - Change the visibility of windows
Algorithm Designer - Launch Algorithm Designer
Downloadable Add-ins Manager - Launch Add-ins manager to install additional modules
Stream Audio - Launch Audio Streaming Window
Project Version Control - Opens the Version Control Window
A/B Testing - Perform blind A/B testing of presets
Settings - Open the settings page
Link - Perform Link operation on the project
Link Compile - Perform link operation and compile the schematics
Link Compile Download - After Link and Compile operations, download the schematic to the target
Clean Link Compile Download - Perform a fresh link compile download by erasing previous data
Export System Files - Export the current project to generate files in the chosen location
Export Preset - Export the presets saved in the project to a separate file
Import Preset - Import the presets saved in a file to apply onto the current project
Enable/Disable Level Detectors - Enable/Disable all Level Detectors
Enable/Disable Continuous Readback - Enable/Disable all Continuous Readback
Content - Launch Help Content for the particular selected item
Index - Launches the SigmaStudio+ landing page
About - Opens a pop-up window displaying details of release and build version along with date and time
Check for Updates - Check and install SigmaStudio+ software updates