The figure above depicts the tabbed document panel. On top, the different tabs which are open are displayed, and below it is the canvas on which the schematic will be designed and implemented. Modules from the toolbox can be dragged and dropped onto the empty canvas. Modules can be dragged in all directions and the canvas scrolls automatically in the direction of drag. The bottom right of canvas has a mini map button which depicts the compressed version of the entire schematic built on the canvas. Using the minimap button the user can scroll to the desired region on the canvas.