This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:sigmastudio [22 Nov 2016 09:21] – Venkatesan Krishnamoorthy | resources:tools-software:sigmastudio [22 Dec 2016 12:32] – [Feature Wishlist] Venkatesan Krishnamoorthy | ||
---|---|---|---|
Line 13: | Line 13: | ||
* To see what SigmaStudio can do, check out the [[resources/ | * To see what SigmaStudio can do, check out the [[resources/ | ||
- | <WRAP important> | + | <WRAP important> |
<WRAP important> | <WRAP important> | ||
Line 67: | Line 67: | ||
[[resources/ | [[resources/ | ||
- | **Bitwise logic support for ADAU170x chip** | ||
- | * Description : SigmaStudio only includes " | ||
- | * Notes : N/A | ||
- | * Developer feedback : | ||
- | |||
- | **Zero phase on VCO ON/OFF command ** | ||
- | * Description : when a VCO is turned OFF, it is simply a switch forcing the output signal to 0. The oscillator keeps running and when the VCO is turned ON, the sinus signal phase is completely random. The zero phase feature should allow the sinus phase to be reset when the switch goes from OFF to ON | ||
- | * Notes : N/A | ||
- | * Developer feedback : |