This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:usingsigmastudio:tcpipchannels [05 Jan 2017 15:36] – [Read Response Format] Ivan Johansen | resources:tools-software:sigmastudio:usingsigmastudio:tcpipchannels [26 Jun 2019 12:08] (current) – TCPIP Added for ADAU146x Sanjeeva Reddy | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======TCP/ | + | ======TCP/ |
[[resources/ | [[resources/ | ||
\\ | \\ | ||
- | |||
The TCP/IP channel can be used to connect with the SigmaDSP in case the SigmaDSP is present at a different location and cannot be physically connected the the PC that is running SigmaStudio. | The TCP/IP channel can be used to connect with the SigmaDSP in case the SigmaDSP is present at a different location and cannot be physically connected the the PC that is running SigmaStudio. | ||
Line 9: | Line 8: | ||
The TCPIP channel is present under the Communication Channels tree as shown in the figure below: | The TCPIP channel is present under the Communication Channels tree as shown in the figure below: | ||
- | {{ : | + | {{ : |
Drag and Drop the channel onto the configuration tab and connect it to the IC. | Drag and Drop the channel onto the configuration tab and connect it to the IC. |