Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:sigmastudio:usingsigmastudio:scripting:create [14 Dec 2016 13:00] – [Opening the Script Editor] TINO TONYresources:tools-software:sigmastudio:usingsigmastudio:scripting:create [02 Jul 2019 13:38] (current) – Added Script Pause and Stop Sanjeeva Reddy
Line 5: Line 5:
 \\ \\
 \\ \\
-SigmaStudio scripts can be created in any text editor or within SigmaStudio using the “Script Editor” tool. The Script Editor provides IntelliPrompt display of the script interfaces and syntax highlighting functionality. Script files can be saved as text files (*.txt) or SigmaStudio Script files (*.sss). Scripts are loaded and run from the Script Editor window.+SigmaStudio scripts can be created in any text editor or within SigmaStudio using the “Script Editor” tool. The Script Editor provides IntelliPrompt display of the script interfaces and syntax highlighting functionality. Script files can be saved as text files (*.txt) or SigmaStudio Script files (*.sss). Scripts are loaded and run, pause, and stop from the Script Editor window. Pause, Resume and Stop supports by adding the "ALLOW_PAUSE_STOP() " API in Script.
 \\ \\
 =====Opening the Script Editor===== =====Opening the Script Editor=====
Line 59: Line 59:
 Figure 4: Script Error Figure 4: Script Error
 \\ \\
 +\\
 +\\
 +=====Pause and Resume a Script=====
 +To pause a SigmaStudio Script, in the Script Editor Window, click on main menu Tools > Pause, see Figure 5.
 +{{ :resources:tools-software:sigmastudio:usingsigmastudio:scripting:pausescript.png?nolink |}}
 +\\
 +\\
 +if the script successfully paused, "Paused" is shown in the Script Editor status bar.
 +Figure 5: Pause Script
 +\\
 +To Resume a SigmaStudio Script, in the Script Editor Window, click on main menu Tools > Resume, see Figure 6.
 +{{ :resources:tools-software:sigmastudio:usingsigmastudio:scripting:scriptresume.png?nolink |}}
 +Figure 6: Resume Script
 +\\
 +=====Stop a Script=====
 +To stop a SigmaStudio Script, in the Script Editor Window, click on main menu Tools > Stop, see Figure 7.
 +{{ :resources:tools-software:sigmastudio:usingsigmastudio:scripting:stopscript.png?nolink |}}
 +\\
 +\\
 +if the script successfully stops, a dialog detailing the script execution halted is displayed and “Script Aborted” is shown in the status bar.
 +{{ :resources:tools-software:sigmastudio:usingsigmastudio:scripting:scriptstopdialog.png?nolink |}}
 +\\
 +{{ :resources:tools-software:sigmastudio:usingsigmastudio:scripting:scriptaborted.png?nolink |}}
 \\ \\
 \\ \\
resources/tools-software/sigmastudio/usingsigmastudio/scripting/create.txt · Last modified: 02 Jul 2019 13:38 by Sanjeeva Reddy