Click here to return to 'SigmaStudio Scripting' page.
Analog.SStudioScripting.IScripted is contained in a .NET assembly, BaseLib.dll, installed in the SigmaStudio folder.
The SigmaStudio application has the capability to run a script from command line. A step-by-step procedure is given below.
1. Open a windows command prompt and change the directory to location of SigmaStudio application “SStudio.exe”.
2. Ensure that there is no other active SigmaStudio application running in the PC.
3. Execute the command “SStudio.exe \script-file Script-file-Name-With-Full-Path”, where “Script-file-Name-With-Full-Path” contains the complete path to the SigmaStudio script.