This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:tools-software:sigmastudio:usingsigmastudio:samplingrateconsiderations [21 Jun 2012 20:39] – [Sampling Rate Considerations] Added information from EZ faq Brett Gildersleeve | resources:tools-software:sigmastudio:usingsigmastudio:samplingrateconsiderations [21 Jun 2012 20:41] – Updated instructions per sample terminology Brett Gildersleeve | ||
---|---|---|---|
Line 5: | Line 5: | ||
\\ | \\ | ||
\\ | \\ | ||
- | The number of instructions available on the DSP (MIPS) | + | The number of instructions available on the DSP per audio sample |
- | * 1536 instructions at 32 kHz | + | * 1536 instructions |
- | * 1536 instructions at 44.1 kHz | + | * 1536 instructions |
- | * 1536 instructions at 48 kHz | + | * 1536 instructions |
- | * 768 instructions at 96 kHz | + | * 768 instructions |
- | * 384 instructions at 192 kHz | + | * 384 instructions |
The sample rate should be set by the program-length bits in the core control register. SigmaStudio defaults to 44.1-kHz sampling, the CD red-book standard. If you want to use another rate, select it prior to your design from the **New Item Sample Rate** drop-down list in the top toolbar. Now any blocks added to your schematic will be set to that sampling rate. | The sample rate should be set by the program-length bits in the core control register. SigmaStudio defaults to 44.1-kHz sampling, the CD red-book standard. If you want to use another rate, select it prior to your design from the **New Item Sample Rate** drop-down list in the top toolbar. Now any blocks added to your schematic will be set to that sampling rate. |