This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudio:usingsigmastudio:linkcompiledownload [18 Jun 2012 20:07] William Jahn created |
resources:tools-software:sigmastudio:usingsigmastudio:linkcompiledownload [14 Jul 2017 14:11] Venkatesan Krishnamoorthy |
||
---|---|---|---|
Line 101: | Line 101: | ||
- | <note tip>Note: When working with evaluation hardware, any time you make edits in the schematic (e.g. add/remove blocks, add/remove wires, add/remove algorithms) you must recompile and download the project before these changes will take effect in the hardware program. If the application status bar does not indicate "Active Downloaded", the downloaded program and schematic design are out of sync.</note> | + | <WRAP tip>Note: When working with evaluation hardware, any time you make edits in the schematic (e.g. add/remove blocks, add/remove wires, add/remove algorithms) you must recompile and download the project before these changes will take effect in the hardware program. If the application status bar does not indicate "Active Downloaded", the downloaded program and schematic design are out of sync.</WRAP> |
- | + | ||
+ | ===== Download Options (ADAU145x) ===== | ||
+ | Link Compile Download will download Regsiters, Program and Data from the schematic. | ||
+ | ==== Register Download ==== | ||
+ | Download of registers can be disabled upon download in the IC Context menu as shown below. | ||
+ | {{ :resources:tools-software:sigmastudio:usingsigmastudio:regdownload.jpg?nolink |}} | ||
+ | |||
+ | ==== PLL Reset ==== | ||
+ | Sometimes user does not want the ADAU145x clock to be reset during download. This can be disabled through the IC Context menu as shown below. After disabling download will not reset the PLL. | ||
+ | {{ :resources:tools-software:sigmastudio:usingsigmastudio:regdownloadd.jpg?nolink |}} | ||
+ | |||
+ | |||