Wiki

This version (30 Jun 2017 11:05) was approved by Venkatesan Krishnamoorthy.The Previously approved version (10 Apr 2017 14:03) is available.Diff

Alias

Add Alias

Right clicking on Input Alias will show option to Add output Alias. That output Alias can be moved to anywhere in schematic and connected with any block as signal destination. One Input Alias can have multiple output Aliases if required.

Highlighting All Alias

Clicking on any Input/Output Alias will highlight All Aliases. Output Aliases will be highlighted in “Aqua” color and Input Alias will be highlighted in “Orange” color.

Go to CounterPart Alias

User can go to particular output alias of choice by using this option. Example: If user clicks “1” in Goto CouterPart Alias option, then “FIR1” block will come into center part of schematic even if it is not in visible area of schematic. This helps user to easily navigate between and evaluate the schematic design.

Go to Input Alias

At any time, user can navigate back to Input Alias from any Output Alias using this option. Goto Input Alias option will be shown in every output alias. After clicking that option, Input Alias block will come into center part of schematic even if it is not in visible area of schematic. This helps user to easily navigate between and evaluate the schematic design.

resources/tools-software/sigmastudio/usingsigmastudio/alias.txt · Last modified: 30 Jun 2017 11:05 by Venkatesan Krishnamoorthy